I want to use one Xbee as coordinator connected to a PC by the USB adapter sold by Sparkfun. That same Xbee, I want to connect to a PicMicro.
Can I use both connections?
Do I have to shutdown, through a switch, one when the other connection is in use?
More details:
I’m setting up a burglar-alarm system.
One Xbee as end device in de barn.
One Xbee as end device in the living-room.
With my question I can decide to buy 1 or 2 Xbees for my workroom.
Through the PC I can set time/date in de barn and other stuff, that needs a change now and then.
Through the PicMicro it’s a alarm function.