I’m having problems with xbee ND frames.
I have multiple routers and end devices connected.
I send (via a coordinator) : 7e 00 04 08 51 49 44 19
I receive : 7e 00 0d 88 51 49 44 00 00 00 00 00 00 00 de ad 0e
Which verifies, both by manual check and because the coordinator didn’t discard it,
I send :7e 00 04 08 52 4e 44 13 (Node discover)
I get back (for example) : 7e 001c 88 52 4e44 00 38cc 0013a200 40ad724c 5230323000 fffe 01 00 c1 05 101e 59
The example module is configured as XB24-ZB, Zigbee router api, firmware 2364.
All the documentation I can find (thanks a lot google) seems to indicate the response should terminate after the NI with the checksum.
Any hints where I can find correct documentation and tutorials?
Thanks in advance
waltr
June 9, 2014, 7:30pm
2
The only documents I have used are directly from Digi International.
http://www.digi.com/support/productdeta … umentation
Thanks. I’ve got that one. After the fact, I can decode the data for the specific example. But there are lots of commands/responses that I need to implement, so I’m hoping for something a bit more concise.
BTW, my target is a Raspberry PI with Arduinos. DIGI seems to only write to a Windows audience. I have XCTU and XCTUng running, with problems, under Wine.
if you can use an arduino environment, there’s an XBee library that supports Xbee S1 and S2 and virtual wire, etc.
waltr
June 10, 2014, 2:09am
5
If using an R-Pi write the frame handling code in Python or C. There are examples for both around.