Hi,
here’s my problem:
I am trying to read an analog Signal (voltage value), digitalise it with the ADC Feature of the XBee.
Then send the digital Signal to a receiving XBee, output it as PWM and run it through a low pass filter to get the original voltage value back.
The problem here is that i don’t get the input value out of the low pass filter. Sometimes i get a voltage that makes no sense (e.g. 2.7V) and sometimes nothing happens.
As i have (or had) not the slightest previous knowledge and experience in these fields, right now i have no clue where i went wrong and would really appreciate your help!
My XBee’s are configured as following:
Sender: (Wiring Diagram: http://sdrv.ms/PzXZqp )
ATID3456 (PAN ID)
ATMY1 (My Adress)
ATDL2 (Destination Adress)
ATD02 (Input 0 in ADC)
ATIR1 (1ms sample rate)
ATIT1 (1 sample before Transmission)
Receiver: (Wiring Diagram: http://sdrv.ms/OnCqVG )
ATID3456 (PAN ID)
ATMY2 (My Adress)
ATDL1 (Destination Adress)
ATP02 (PWM 0 in PWM mode)
ATIU1 (I/O Output enabled)
ATIA1 (I/O Output from adress 1)
I really hope you can help me out ![]()
Greets
Lars