Hi folks,
I’d like to set a breakpoint in a kernel I don’t have source code for, as I am just trying to see how it initializes some hardware… ie pci.
I have an Olimex Arm-Usb-OCD, and I have used OpenOCD v728 for most of my time with OpenOCD. Yesterday I pulled rev 1192 from svn. Whew! It has changed alot! Xscale support has improved. I’ll just name 2 items… but there are more.
xscale debug_handler
xscale vector_catch
I hope those 2 new additions can help me do what I need to do. I believe I have it setup correctly. It detects my flash chip, and I have working_area setup to speed things up a bit. ![]()
When I get the target halted, with pc=0, and then do a resume, it will proceed for a bit but inevitably gets stuck with pc=0xffff0018. At that point the mmu, D-Cache, I-Cache are also enabled by that kernel.
Documents I have found that discuss what may be happening here.
www.arium.com/support/pdf/XScale_app_note.pdf
http://www.webetools.com/ultsol/users/k … d=39&sid2=
Dominic Rath’s master_thesis.pdf ‘out there’ mentions some of the inabilities of open source debuggers and mmu units. (I hope what he says there is still not the case!)
In openocd/src/target/xscale.c line 1735 it appears to use some hard coded locations… at 0x0 and 0xffff0000 in calls to xscale_load_ic but that may be insignificant.
I guess I should also mention this is an older 2.4 kernel.
I hope that I can get around this, even if I have to set some memory watches at the vector tables and do some fudging to make sure the mini ic is in agreement with the system.