Hi!
I have the M8Q , i have tried change /save settings in U-center and it works. But after powerloss (empty battery) the settings is back to “default” . I thought m8q had a non-volatile memory for keeping the settings permanent. Do i need a add-on card to be able to have my gps settings permanent stored ?
/Mattias
I’d guess that the on-board battery that enables saving is discharged; see the section about ‘Battery’ here https://learn.sparkfun.com/tutorials/sp … 1643964608 and perhaps leave the board powered for a day or so to fully re-charge the battery?
Hi! Yes thats my problem, i want the settings to be permanent without the battery even being connected. But then it requires some sort of flash memory i guess. But i thought a non-volatile memory would hold the settings permanent even if the battery would drain.
/Mattias