I noticed that the 0805 package in SparkFun library appears to be smaller than the default 0805 packages. Since it is likely that there are lots of people using the SparkFun package, without problem, does anyone know why it is different? It is also missing the Keepout layer.
The only reason why I noticed is because I’m making my own library (I used the footprint from a datasheet from Murata) and when I replaced the SF part with my part, it didn’t match. But my part matches the default package.
The 0603 package is identical to the default package and includes the Keepout layer - only the 0805 seems to be different.