1-Wire IOIO Board

Hi friends,

I have a BIG problem.

I bought a DS18B20 , but i dont know uses it, so I researched on the internet it uses a form of data transfer call 1-wire.

It is possible to read this sensor using the IOIO board - OTG?

Is there another way to use this sensor without using 1-wire?

Can you help me?

Thank you.

http://lmgtfy.com/?q=interface+ds18b20

I have done some research, many say it’s not possible.

Can someone help me? Are you doing this?

You got the first link that appeared and copied here? lol

As I said, well researched … 've Seen this solution however it does not use a sensor with 1-wire protocol, it uses the TMP36.

Can someone help me? I need to use the specific sensor DS18B20

Considering that it showed up on the first page I searched, pretty much. http://www.briandorey.com/post/Raspberr … ogger.aspx

Anyway, I’m not posting to be snarky. The 1-Wire protocol is well documented and there is tons of source code all over the net to use it. You just have to modify it for IOIO.

(for the confused: I posted a link and deleted it because I was called away before I could update it with the correct information).

Everything I understand, however nothing is as simple as that … rs

Especially when dealing android sending commands to the ioio, it lost a few milliseconds …

the one given here, the own Ytai spoke q is tense …

https://groups.google.com/forum/ #! msg/ioio-users/C0dvHHsQQM4/a2MSWGN7H3QJ

= D