130-200mhz Lora boards?

Hi All,

Anyone know if sparkfun do any low frequency LORA boards? I’m looking for something 100-200MHz.

I’ve looked around but can see anything. Most are of course tuned for the standard LORA bands so not surprised. However, a number of the semtech and hoperf chips are capable of sub 200mhz.

Sparkfun’s LoRa modules are of higher frequencies. For 100 MHz, you can see this. https://www.aliexpress.com/i/1005008096781206.html

Can you please choose one that isn’t 105.9 MHz? My local news station broadcasts sports coverage on that channel and I don’t want to miss any scores.

And not on 156.180 MHz, our Fire Department dispatches there. But 155.805 is good, that’s the next town over and we’re hockey rivals. They suck, we beat them almost half the time.

Come to think of it, shoot, not on 121.5 MHz, either, at least till I get back from my trip. That’s the international guard frequency used for vessels in distress. Airport tower dispatch frequencies are OK, controllers can use semaphore or landing light blinks to communicate the emergency.

Yup, @brow won the internet for today.

Haha nice. 450mhz-ish is pretty good for turning in everyone’s lights and ceiling fans. Amusing at 3am…