SparkFun LoRa Gateway - 1-Channel (ESP32) EU 868 MHz band support

Hello. I am planning to by a SparkFun LoRa Gateway - 1-Channel (ESP32) to be used in Europe. From the doc it is not clear if the product can only work at 915 MHz or if it can also be configured to use the EU 868 MHz band. Could you please tell me if I would be able to configure the board to use the EU 868 MHz band if I buy such a board. Thanks in advance for your answer. Regards,

yes… it works on 868 in Europe as well…