ESP_sc_gway - setup for Australia

Hi - I’m new to this, so please be gentle.

I have a pair of Sparkfun Lora Gateway-1-ch(ESP32) which I’m trying to configure.

I have followed the hookup instructions and now have 1 board configured as a gateway (on wifi - serving a webpage)

The other board is configured as a device - showing period transmissions - see below

1097454844: engineUpdate, opmode=0x808

1097454866: Unknown event

1097454868: engineUpdate, opmode=0x888

1097454933: TXMODE, freq=905700000, len=26, SF=7, BW=125, CR=4/5, IH=0

Packet queued

1097521196: setupRx1 txrxFlags 0x20 → 01

start single rx: now-rxtime: 4

1097521327: RXMODE_SINGLE, freq=923900000, SF=7, BW=500, CR=4/5, IH=0

rxtimeout: entry: 1097521412 rxtime: 1097521321 entry-rxtime: 91 now-entry: 4 rxtime-txend: 62524

1097584056: setupRx2 txrxFlags 0x1 → 02

start single rx: now-rxtime: 3

1097584187: RXMODE_SINGLE, freq=923300000, SF=9, BW=125, CR=4/5, IH=0

rxtimeout: entry: 1097585484 rxtime: 1097584181 entry-rxtime: 1303 now-entry: 3 rxtime-txend: 125384

1097585500: processRx2DnData txrxFlags 0x2 → 00

1097727762: processDnData txrxFlags 00 → 20

1097727765: EV_TXCOMPLETE (includes waiting for RX windows)

1097727768: engineUpdate, opmode=0x800

Specific questions - how do I interpret this output?

Line 4 looks like it is transmitting (TXMODE) on 905700000 len 26 , SF 7 BW 125 kHZ - where is that frequency set?

so I assume this is transmitting 26 bytes (? including the ‘hello world’ message plus some meta data)

the rest looks like receive window data

Rx 1 is waiting for data on 923900000 with SF7

Rx 2 is waiting for data on 923300000 with SF9

is that correct?

lmic_project_config.h looks like this

// project-specific definitions

//#define CFG_eu868 1

#define CFG_us915 1

//#define CFG_au921 1

//#define CFG_as923 1

// #define LMIC_COUNTRY_CODE LMIC_COUNTRY_CODE_JP /* for as923-JP */

//#define CFG_in866 1

#define CFG_sx1276_radio 1

//#define LMIC_USE_INTERRUPTS

#define LMIC_DEBUG_LEVEL 2

ESP-1CH-TTN_DEVICE_APB has the following modifications (as per instructions)

Const lmic_pinmap (as per the hookup notes)

BUT *******

Where the hookup notes say // first diable all sub-bands

// First disable all sub-bands
for (int b = 0; b < 8; ++b) {
  LMIC_disableSubBand(b);
}
// Then enable the channel(s) you want to use
LMIC_enableChannel(8); // 903.9 MHz

My code says

  // First disable all sub-bands
  for (int b = 0; b < 8; ++b) {
    LMIC_disableSubBand(b);
  }
  // Then enable the channel(s) you want to use
  //LMIC_enableChannel(8); // 903.9 MHz
  LMIC_enableChannel(17);
#endif

I don’t understand this bit at all - (not got my head around the channel numbers - doesn’t seem to relate to anything I’ve found online)

What channel do I want to use for Australia?


The gateway is configured ( as per the instructions ) - like this

Version = V.5.3.3.H; 180825a

ESP-sc_gway.h TAB

DUSB 1

_LFREQ 915

_SPREADING SF9

_CAD 0

_PIN_OUT 6

_STRICT_1CH 0

CFG sx1276 radio

(all the WiFi and TTN are configured and ? working)

loraModem.h TAB

struct pins { etc has been copied and inserted as per instructions)

Int freqa array looks like this

int freqs [] = { 
	868100000, 									// Channel 0, 868.1 MHz/125 primary
	868300000, 									// Channel 1, 868.3 MHz mandatory
	868500000, 									// Channel 2, 868.5 MHz mandatory
	867100000, 									// Channel 3, 867.1 MHz Optional
	867300000, 									// Channel 4, 867.3 MHz Optional
	867500000,  								// Channel 5, 867.5 MHz Optional
	867700000,  								// Channel 6, 867.7 MHz Optional 
	867900000,  								// Channel 7, 867.9 MHz Optional 
	868800000,   								// Channel 8, 868.9 MHz/125 Optional
	869525000									// Channel 9, 869.5 MHz/125 for RX2 responses SF9(10%)
	// TTN defines an additional channel at 869.525Mhz using SF9 for class B. Not used
};
#elif _LFREQ==433
// The following 3 frequencies should be defined/used in an EU433 
// environment.
int freqs [] = {
	433175000, 									// Channel 0, 433.175 MHz/125 primary
	433375000, 									// Channel 1, 433.375 MHz primary
	433575000, 									// Channel 2, 433.575 MHz primary
	433775000, 									// Channel 3, 433.775 MHz primary
	433975000, 									// Channel 4, 433.975 MHz primary
	434175000, 									// Channel 5, 434.175 MHz primary
	434375000, 									// Channel 6, 434.375 MHz primary
	434575000, 									// Channel 7, 434.575 MHz primary
	434775000 									// Channel 8, 434.775 MHz primary
};
#elif _LFREQ==915
// US902=928
// AU915-928
int freqs [] = {
	// Uplink
	903900000, 									// Channel 0, SF7BW125 to SF10BW125 primary
	904100000, 									// Ch 1, SF7BW125 to SF10BW125
	904300000, 									// Ch 2, SF7BW125 to SF10BW125
	904500000, 									// Ch 3, SF7BW125 to SF10BW125
	904700000, 									// Ch 4, SF7BW125 to SF10BW125
	904900000, 									// Ch 5, SF7BW125 to SF10BW125
	905100000, 									// Ch 6, SF7BW125 to SF10BW125
	905100000, 									// Ch 7, SF7BW125 to SF10BW125
	904600000 									// Ch 8, SF8BW500 
	// Downlink
	// We should specify downlink frequencies here											
												// SFxxxBW500
};
#else
int freqs [] = {
	// Print an Error, Not supported
#error "Sorry, but your frequency plan is not supported"
};
#endif
uint32_t  freq = freqs[0];
uint8_t	 ifreq = 0;								// Channel Index

I’m not sure if I’m supposed to comment any of these out or not?

Both sketches compile and upload fine - the gateway webpage runs - and shows the following settings

CAD = ON

HOP = OFF

SF Setting = AUTO

Channel = 0

WWW Refresh = ON

The message History shows 1 message (which I don’t think was me - but I don’t know for sure)

Saturday 26-9-2020 03:53:55 4f c5 dd 72 0 903900000 7 -118

Now I’m stuck as to what to do next.

My device appears to be transmitting (both have antenna by the way) - as per the Tx example shown above - but I’m not seeing any activity on the webpage at all (apart from the regular refresh).

So - specific questions

What channel (and other) settings should I use for Australia

Where can I find something more specific on how channels relate to frequencies (what Ch no. os which frequency? - Is that just the centre frequency? (I assume it is)

Should I expect to see any received messages on the webpage - or should I add a serial port

I’m sure many other beginners have had the same or similar questions - please don’t assume I know ANYTHING when answering any of this - your answers could help many people.

Many thanks in advance