For my project, I have 2 4V Lipo Batteries in series with a 5V regulator (detailed in BatteryBoard.png). I would also like to charge these batteries with a Lipo Charge Plus. I have tried connecting the batteries in series using the + and - on the lipo charger board. However, at the end of my circuit I only get 4V instead of 8, indicating that the batteries are somehow in series. I am assuming that it has to do with the grounding. I have also tried connecting the batteries in series before the lipo charger making it only necessary to have 1 Lipo Charger and I got a readout of 8V (1Charge.png). But this setup does not allow me to charge the batteries because the maximum regulated output voltage for the lipo charger plus is 4.232 V and with the batteries in series it would be too much for the microcontroller on the lipo charge plus.
Is there any way that I can put these batteries in series for my circuit as well as charge them?
I would really like to have the original design but I do not know how to make it so that the batteries are not in series.