315 Mhz vs 434 Mhz

What are the advantages and/or disadvantages between the 315 MHz and the 434 Mhz RF Link Transmitters and Receivers available from SFE?

315 Mhz Receiver: http://www.sparkfun.com/commerce/produc … ts_id=8947

434 Mhz Receiver: http://www.sparkfun.com/commerce/produc … ts_id=8950

Also, can someone confirm the supply voltage required for either of the 4800 bps receivers? The data sheet(http://www.sparkfun.com/datasheets/Wire … RX3400.pdf) says 4.5V-5.5V. but the KLP_Walkthrough(http://www.sparkfun.com/datasheets/RF/K … hrough.pdf) shows 3.3V-6V.

thanks.

patrick

It depends on the country where they are used. For instance, 434 MHz is legal in the UK.

Leon

315 will have better penetration into non metal structures, but the antenna is longerby 25%. 434 is more line of sight.