in both binary and acii output of the yaw gyro does not work (P0.15).
in ascii is is around value 264 and it looks like it is floating becouse it reacts a littlebit on action with the roll gyro. but it doesn’t do anything with the yaw gyro like it should do.
when i measure on pin P0.15 i see the yaw gyro does work, and gives proper values when moving, and is in de same range like the other gyro’s
so, i am sure the yaw gyro works.
also try’d to remove the sensor board.
and test if the gyro pins (P0.12, P0.13, P0.15) value go to zero when connected to ground.
now running without sensor board, all gyro values are floating around ~255,
when connection with ground, Pitch and roll values get zero, but yaw still is ~255
so, i am now pretty shure something is wrong with the lpc2138 micro controller. and could be as simple as something wrong with flash image, or some devices on the chip not properly initialised.
I got the 6dof v4 sensor just 1 day ago, and didn’t do any programming or flash things yet.
but still, what do you think
is pin P0.15 broken? is it possible for a new device.
or did anyone else experience something simular?
or other suggestions?