802.15.4 to communicate with 802.11b

can the zigbee specification communicate with 802.11b? that is, can a XBee device communicate with a Lantronix Matchport device?

IEEE 802.3 is not TCP/IP

and vice versa

IEEE 802.11 is not WiFi

and vice versa

IEEE 802.15.4 is not ZigBee. (ZigBee is a peer of the IP protocol)

and vice versa

IEEE 802.15.4 is not ISA 100.11a

and vice versa

Belatedly, answer to posted question:

No, IEEE 802.15.4 is a totally different MAC and PHY than is IEEE 802.11. '15.4 is a 2MHz bandwidth signal and 802.11 is 20MHz wide. And the modulation methods in each are not similar.

Didn’t think so. Just curious, are there bridges that can bridge the two in a mixed environment?

thanks for the reply

Ready made bridges may exist, but ZigBee doesn’t have a standardized protocol for the trunking to IP networks.

If you’re really looking for a bridgeable type network, ISA 100 defines this pretty well, as well as 6LoPan (IPv6 over 802.15.4)

rdxbam:
Didn’t think so. Just curious, are there bridges that can bridge the two in a mixed environment?

thanks for the reply

Yes, look on Digi’s website

The ConnectPort gateways from Digi are great, however depending upon your application they may be way too expensive.

Another option is to create a simple gateway. Get a WiPort or MatchPort module from Lantronix and route the serial output of the XBee to the serial input of the Lantronix module. Configure the Lantronix module to automatically connect to a particular IP address and port. Now everything addressed to that XBee will automatically be repeated over the Internet.

Alternately, you could plug one XPort into your computer and write a simple program to either directly repeat the serial traffic, or process it locally before sending modified information along.

thanks all & Faludi, i’ll delve more into the simple gateway which would be more cost effective for our situation it would seem. thanks for the tip on 6LoPan, i’ll look into that more also.