Hi everybody! Sorry for my orrible English…it’s not my first language :oops:
However, I’m in trouble with mi Olimex Arm-usb-ocd, because, every time I connect it for programming and debuggin my LPC1768 board, openocd gives me this output:
@eg-AO725:~/Embedded_System/First$ sudo openocd -f sr/share/openocd/scripts/interface/olimex-arm-usb-ocd.cfg -f /usr/share/openocd/scripts/target/lpc1768.cfg
Open On-Chip Debugger 0.6.1 (2013-01-24-00:06)
Licensed under GNU GPL v2
For bug reports, read
http://openocd.sourceforge.net/doc/doxygen/bugs.html
Info : only one transport option; autoselect ‘jtag’
adapter_nsrst_delay: 200
jtag_ntrst_delay: 200
trst_and_srst srst_pulls_trst srst_gates_jtag trst_push_pull srst_open_drain
adapter speed: 500 kHz
Info : clock speed 500 kHz
Info : inter: 0.000221, inter2: 0.000222 end: 0.002824
Info : JTAG tap: lpc1768.cpu tap/device found: 0x4ba00477 (mfg: 0x23b, part: 0xba00, ver: 0x4)
Info : inter: 0.000220, inter2: 0.000221 end: 0.001731
Info : inter: 0.000902, inter2: 0.000904 end: 0.001536
Info : inter: 0.000497, inter2: 0.000498 end: 0.001442
Info : inter: 0.000658, inter2: 0.000660 end: 0.001596
Info : inter: 0.000285, inter2: 0.000286 end: 0.001687
Info : inter: 0.000269, inter2: 0.000271 end: 0.001624
Info : lpc1768.cpu: hardware has 6 breakpoints, 4 watchpoints
Info : inter: 0.000608, inter2: 0.000609 end: 0.001387
Info : inter: 0.000198, inter2: 0.000199 end: 0.003225
Info : inter: 0.000519, inter2: 0.000520 end: 0.001633
Info : inter: 0.000321, inter2: 0.000322 end: 0.002552
Info : inter: 0.003733, inter2: 0.003734 end: 0.003996
Info : inter: 0.000512, inter2: 0.000513 end: 0.001803
Info : inter: 0.000204, inter2: 0.000205 end: 0.002233
Info : inter: 0.000258, inter2: 0.000259 end: 0.002250
Info : inter: 0.000776, inter2: 0.000777 end: 0.002338
Info : inter: 0.000246, inter2: 0.000247 end: 0.002225
Info : inter: 0.000207, inter2: 0.000209 end: 0.001421
Info : inter: 0.000253, inter2: 0.000254 end: 0.001436
(this continues until I shut down openocd or I write “reset halt” via telnet)
I use a pipe with telnet for comunicate with openocd, and telnet gives me the same outputs (but in telnet I can give command).
I need your help because I don’t understand this output. I see that in another computer (another users :roll: ) this not appear.
I use openocd 0.6.1 and my openocd.cfg is that:
telnet_port 4444
gdb_port 3333
tcl_port 6666
interface ft2232
source [find interface/olimex-arm-usb-ocd.cfg]
source [find target/lpc1768.cfg]
what is the problem??
EDIT: I see that is not a problem using gdb, because I can load a binary file on the lpc1768 and set the break…so, what is this strange info???