In Aug 2022, I ordered one soldering iron through Digikey:
https://www.digikey.sg/en/products/deta … VzCS%2BgyA
It works great, with the line voltage of 220V in Singapore.
When I try to re-order it today (with the same digital key number), I found the line voltage specified is 110V only.
Q1: For the soldering iron sold in 2022, is it rated at 110V or 220V?
If it is 110-V only, how can I use it in Singapore (220V) directly?
Q2: For the soldering iron currently available, can you help check whether 220V is supported?
Many thanks.