Hi all,
The Olimex CS-E9302 was designed without sound output devices.
But the board have two strong USB ports, I want to use the USB port
for USB sound device. Which USB devices are compative with EP9302 and the right drivers ?
I’m using linux-2.6.24-rc8 kernel and the Ivanov Debian rootfs.
Thanks
Hello,
I search the Kernel linux 2.6.24 rc8.
does this properly function? it is supported mmc/sd? Can you send him to me? (upload)
THX
Chris
chris233:
Hello,
I search the Kernel linux 2.6.24 rc8.
does this properly function? it is supported mmc/sd? Can you send him to me? (upload)
THX
Chris
CS-E9302 + ivanov arm debian rootfs
—> I stored rootfs in USB flash disk and it worked OK, it very simple.
use the following kernel command line:
exec -c "console=ttyAM root=/dev/sda1 rootdelay=5".
please visit my page : http://kamejoko80.wikidot.com/arm
Please patient about my pour English!