I have just purchased an Olimex CS-E9302 Development Board and I was wondering if anyone could point me in the right direction on downloading a prebuilt, or building a linux kernel that supports the Ethernet, USB, Serial, SD Card, aswell as the FAT32 filesystem for USB Drives and FTDI USB/Serial device drivers (for my USB CrystalFontz CFA635)
Well, I have built myself a 2.6.22.1 kernel with most of the stuff I want. I found an SSP/SPI driver for the E9301/E9302 processors, and I just gotta put together an MMC host driver for the Olimex CS-E930x boards which shouldn’t be too hard, linux drivers are much easier than windows.