We are using an AD8232 to obtain an ECG signal.
We are using a 3-lead setup and have attached the leads to the arm, to the arm & thigh, and to the abdomen, in the 3 most common configurations seen online, on 3 different people. We have tried changing which leads were in which positions, and incrementally adjusting them at the given sites.
We were initially powering with a laptop and Arduino, but then learned about the possibility of 60Hz noise, so we switched to using a DC power supply and examining the output signal with an oscilloscope.
No matter whether the electrodes are touching skin or just air, the oscilloscope shows an intermittent square wave from 0 to 3.2V, as seen on the attached image. Changing the lead positions has no effect whatsoever on the waveform: the value is always either 0 or 3.2V.
We suspect the board is defective. Any suggestions?