ADXL355 Accelerometer latency on output

What is the delay or latency between the input and output in the ADXL355 Accelerometer?

Hi valter92,

Since this is an analog accelerometer, the latency is going to be extremely low. Any significant delay in this would be created by the controller it is attached to. The tuning capacitors we populate on this board sets the bandwidth to 50Hz but you can theoretically get up to 1600Hz on the X and Y axes and 550Hz on the Z axis. For more information on that, I would recommend reading through the [datasheet for the ADXL335.](https://www.sparkfun.com/datasheets/Components/SMD/adxl335.pdf)