I submitted a design, and I’m worried about the drill drawing.
Altium 9 generates Gerber drill drawings with GD1 and GG1 file names, neither of which BatchPCB will accept. If I generate an “NC drill file” named DRL, when I upload it to BatchPCB, I get a “You have not selected a drill file” message. If I click Continue, the board does pass the Design Check. Is everything OK or am I going to run into problems later? The confirmation email didn’t include any kind of drill drawing attachment.
I only do this every couple of years, so I forget…
jimg:
I submitted a design, and I’m worried about the drill drawing.
Altium 9 generates Gerber drill drawings with GD1 and GG1 file names, neither of which BatchPCB will accept. If I generate an “NC drill file” named DRL, when I upload it to BatchPCB, I get a “You have not selected a drill file” message. If I click Continue, the board does pass the Design Check. Is everything OK or am I going to run into problems later? The confirmation email didn’t include any kind of drill drawing attachment.
I only do this every couple of years, so I forget…
If you don’t submit a drill file, I think you’re going to get a board with no holes drilled in it. I would like to know the solution to this problem as well, since BatchPCB doesn’t recognize my NC Drill files from Altium 10 either.
Edit: Figured it out. The .DRL file that Altium generates is a binary file, while BatchPCB expects an ASCII drill file. Luckily Altium also generates this! For me it comes out with a .txt extension. Just rename it to .drl or .drill and BatchPCB should pick it up.
If the Altium users here are in need of more assistance, I’d be willing to take some photos/screenshots or send along pieces of the Altium project if it helps (i.e. output jobs you can import or a whole project to get the gist).
Every standard component package in the world is already built in - With some practice, you can bang out a board in altium from schematic in about 30-60 minutes, have a 3D model generated, gerbers, and even bill of material lists showing all your part numbers, prices exported right to Excel to give you a total cost.
(I’ve started projects on a Monday and had a fab’d board from China in my hand the following Monday)
I also recommend using gerbv to check the output - just ensure the holes line up with the pads.
Its both a hobby and a job for me - and this software is some of the best packages I’ve ever used.