AmbiqMicroDataTransferProtocolServer amdtps sdk 2.3.2 BLE -> Android Phone <--> Arduino Core 1.0.29

AMDTPS-PortSDK-2.3.2-toArduino-Core-1.0.29-Modified-wth-SDK2.3.2-files

amdtps example fully compile-able in Arduino core using 1.0.29 modified with SDK2.3.2 files. IT WORKS.

Phone app, batch install file, Arduino sketch files, platform.txt file, and instructions are in Github repo:

https://github.com/kerryeven/AMDTPS-Por … .3.2-files

Does require manual install of AmbiqSuiteSDK 2.3.2 but no SDK knowledge is required once that is done.

  • fixes pwm issues with SDK 2.2.0

  • fully implements features of the data transfer protocol, including security functions

  • does Send / Receive using Play Store Nrf Connect if you use TEXT format data

just tried with 2.4.2SDK…works as well so should probably jump right to that.

https://www.ambiqmicro.com/mcu/

Scroll to Apollo3 Blue select software then AmbiqSuite SDK Version 2.4.2 and unzip to c:/Users/YourName/Documents then runt the makesdk.sh