I am trying to install OpenOCD with the Amontec JTAGkey but are not having any success. Any help is appreciated!!! ![]()
I have installed the libftd2xx.so.0.4.10 library from Amontec (and can see it with ldconfig -p |grep libftd2)
I can see the Amontec USB device with USB view and can see them in /proc/bus/usb/devices …
T: Bus=01 Lev=02 Prnt=04 Port=03 Cnt=01 Dev#= 9 Spd=12 MxCh= 0
D: Ver= 2.00 Cls=00(>ifc ) Sub=00 Prot=00 MxPS= 8 #Cfgs= 1
P: Vendor=0403 ProdID=cff8 Rev= 5.00
S: Manufacturer=Amontec
S: Product=Amontec JTAGkey
S: SerialNumber=32Q1Q4X9
C:* #Ifs= 2 Cfg#= 1 Atr=80 MxPwr=100mA
I:* If#= 0 Alt= 0 #EPs= 2 Cls=ff(vend.) Sub=ff Prot=ff Driver=(none)
E: Ad=81(I) Atr=02(Bulk) MxPS= 64 Ivl=0ms
E: Ad=02(O) Atr=02(Bulk) MxPS= 64 Ivl=0ms
I:* If#= 1 Alt= 0 #EPs= 2 Cls=ff(vend.) Sub=ff Prot=ff Driver=(none)
E: Ad=83(I) Atr=02(Bulk) MxPS= 64 Ivl=0ms
E: Ad=04(O) Atr=02(Bulk) MxPS= 64 Ivl=0ms
I built openocd (svn) with
./configure --enable-ft2232_libftd2xx
when I run openocd I get the following errors…
# openocd -f OpenOCD-ARM926EJS.config
Open On-Chip Debugger 1.0 (2008-07-12-14:38) svn:799
$URL: svn://svn.berlios.de/openocd/trunk/src/openocd.c $
Error: jtag.c:1689 handle_interface_command(): No valid jtag interface found (ft2232)
Error: jtag.c:1690 handle_interface_command(): compiled-in jtag interfaces:
Info: options.c:50 configuration_output_handler(): Runtime error, file “?”, line 8:
Info: options.c:50 configuration_output_handler(): No valid jtag interface found (ft2232)
compiled-in jtag interfaces:
Info: options.c:50 configuration_output_handler(): In procedure ‘unknown’ called at file “?”, line 1
Info: options.c:50 configuration_output_handler(): In procedure ‘interface’ called at file “OpenOCD-ARM926EJS.config”, line 7
Info: options.c:50 configuration_output_handler(): Runtime error, file “?”, line 8:
Info: options.c:50 configuration_output_handler(): No valid jtag interface found (ft2232)
compiled-in jtag interfaces:
Runtime error, file “?”, line 8:
No valid jtag interface found (ft2232)
compiled-in jtag interfaces:
In procedure ‘unknown’ called at file “?”, line 1
In procedure ‘interface’ called at file “OpenOCD-ARM926EJS.config”, line 7
Info: options.c:50 configuration_output_handler(): In procedure ‘unknown’ called at file “?”, line 1
Info: options.c:50 configuration_output_handler(): In procedure ‘interface’ called at file “OpenOCD-ARM926EJS.config”, line 7
Info: options.c:50 configuration_output_handler(): In procedure ‘unknown’ called at file “?”, line 1
Info: options.c:50 configuration_output_handler(): In procedure ‘script’ called at file “?”, line 1
It seems that it cannot see the JTAGkey. I don’t think it’s a permission problem because I’m running as root.
This is my config file:
# Reference: http://openfacts.berlios.de/index-en.ph … figuration
OpenOCD daemon configuration
telnet_port 4444
gdb_port 3333
#interface
interface ft2232
ft2232_device_desc “Amontec JTAGkey”
Cannot use device descriptor AND serial number
ft2232_serial “32Q1Q4X9”
ft2232_layout jtagkey
The Amontec JATGkey has the VID & PID as shown
ft2232_vid_pid 0x0403 0xcff8
Try maximum speed
jtag_speed 0
use combined on interfaces or targets that can’t set TRST/SRST separately
reset_config trst_and_srst
jtag scan chain
format L IRC IRCM IDCODE (Length, IR Capture, IR Capture Mask, IDCODE)
jtag_device 4 0x1 0xf 0xe
jtag_nsrst_delay 200
jtag_ntrst_delay 200
#target configuration
daemon_startup attach
#target (run for 1 second then halt after a reset. Possible options are reset_halt, reset_run, reset_init, run_and_halt, run_and_init
target arm926ejs little run_and_halt 1