The best solution is to emulate the big expensive liquid fuel rockets that fly to orbit with super expensive payloads…
Run your antennas feedlines from the radios to the appropriate locations on the rocket body where your multiband dipoles are strung parallel to the rocket body. These signal feeds would be proper shielded mini coax from the SMAs or whatever interface jack the radios have, minimizing line loss and making the link to the antennas as neutral to affecting vSWR as possible, so that the Coms link performance is mostly determined by how accurately you phase and match the antenna array.
Now, the antennas are 1/2 wave dipoles with the counterpoise (virtual ground) section of the dipole is above the antenna feed point. The driven element extends down the rocket body from the antenna feed point in the opposite direction.
Since the body as metallic, Use 10mm rubber standoffs to separate the dipole elements from the rocket body.
This will naturally create a directional condition with signal gain existing on the side of the rocket with the antenna.
So then you use the fins to spin the rocket real fast so you now can get rapid blips of telemtry synchronized by the Roll axis rotation rate…;0)
no. kiddings…
You phase together two more Dipoles of the same common feed line forming a tuned array of 3 diploles 120 degrees apart.
Do the same methodology on any other RX/TX subsystems onboard, feeding RF to location of dipole feed points with shielded coax right into open radiating elements positioned the same way…if only two feeds (I/O) to two onboard radio subsystems needed, it would be one band operating via tri-phased rocket body dipoles(3) 120 degrees separation, and the other antenna array for the 2nd feed just laid out the same way but out-of-phase 60 degrees (in relation to the 1st array’s locations) so both antenna arrays share congruent placement around the rocket body exterior, with no blind spots and minimal fluctuation. Each 60 degrees around the body you have a dipole from one of the two arrsys mounted parallel to the body, and with driven elements facing “retrograde” (back at earth) during flight…the next 60 degrees around is a dipole from the other array, with this alternating arrangement.
This provides basically a vertical polarized antenna system you can use with verticals on the ground station, or some directional Yagi’s (recommended anyway) arranged with vertical polarization mounting for GS…or, co-phase the Ground Station antennas (vertical, plus the directional Yagis also) for tracking diversity , or rapid-switch between omni directional and directional segments during flight depending on need.,.
One other method would be to employ LHCP or RHCP polarization and rout the antennas “around” a desired location of rocket body (cork-screw) with a mounting arrangement winding around the rocket body 'no tighter than 30 degrees pitch, leaving enough separation from itself to allow maximal tuning potential (lowest vSWR we can get).
Paying attention to whether the onboard antennas are wound right hand or left hand polarized orientation, matching this with RHCP or LHCP (? hand circular polarized) antennas. These can be aimed directionally at the rocket also, like a beam Yagi for enhanced signal quality, or can be static mounted and used as omni directional antennas.
I would lean toward the dipole orientation arranged as described with counterpoise elements facing toward the nose, and drivens facing earth.
AS long as you give the elements some non-conductive stand-offs (10mm should do) SWR results with both antenna arrays for both radio subsystems operating at same time should be more than acceptable…in fact, they should provide tuning latitude to allow both your antenna arrays quite exceptional tuning potentials, with very low vSWR at the radios onboard.
The key here is feedline quality, matched to a carefully measured dipole array sporting decent SWRs (or as good as can had). The math can be kinda hairy constructing a tri-phased dipole array, theres a deviation in there that makes each singular dipole by itself high SWR (out of tune for single operation by itself) , but when you get that common length just right its magic.
Signal propagation from tri-phased vertical polarized dipole arrays it excellent in most cases.
One of my alltime favorite homebrew antennas for Ham radio has been tri-phasing 3 longwire dipoles with 3 feedlines, each dipole singularly tuned for standalone operation, and using a 3-into-1 antenna switch (mine were homemade with toggles) so you can choose Omnidirectional operation with all 3 being used at once, or selecting single diploes to use facing the direction of the target station, boosting performance by emulating a type of beam antenna with the two unused segments of the array acting as passive reflectors. Fun and easy little arrangements thay can be, like having a directional setup without all the cost and trouble of having a tower installation and Beams antennas to aim.
Anyway, that was slightly off topic, butr wanted to express the confidence of this arrangement while phased.