any way to receive the data from the GPS module

Am doing a project using the GPS Module. the main scenario is to display the position of the object in the maps.

Scenario : there should be an GPS module and the GPS data receiver. the receiver will get data from the GPS module and store in our database. and there is a application to view the data on map.

Issue: how i can receive the data from the GPS module, and whats the receiver should be??? no GPRS or bluetooth Chip in the GPS module, Is there any signal we can use to get the data from the GPS module?? :think:

All independent GPS modules that I know of provide output on a TTL serial connection. With a TTL serial to USB adapter, e.g. http://www.sparkfun.com/products/718 (mind that the correct 3.3 V or 5.0 V IO option is chosen) you can then read the output with just about any computer or USB-enabled handheld device.