Arduino EasyVRShield can't read?? Need help!

Hi all. i have created a mini project whereby i can control the lights of the leds and fans to turn on and off with my voice command. But the problem now is, now that i have train all my commands, when i say them after putting the pin to SW mode, the board does not read me. Can anyone explain why?

#if defined(ARDUINO) && ARDUINO >= 100
  #include "Arduino.h"
  #include "SoftwareSerial.h"
  SoftwareSerial port(12,13);
#else // Arduino 0022 - use modified NewSoftSerial
  #include "WProgram.h"
  #include "NewSoftSerial.h"
  NewSoftSerial port(12,13);
#endif

#include "EasyVR.h"
EasyVR easyvr(port);

//Groups and Commands
enum Groups
{
  GROUP_0  = 0,
  GROUP_1  = 1,
};

enum Group0 
{
  G0_CLOVER = 0,
};

enum Group1 
{
  G1_RED_ON = 0,
  G1_GREEN_ON = 1,
  G1_YELLOW_ON = 2,
  G1_RED_OFF = 3,
  G1_GREEN_OFF = 4,
  G1_YELLOW_OFF = 5,
  G1_RED_BLINK = 6,
  G1_GREEN_BLINK = 7,
  G1_YELLOW_BLINK = 8,
  G1_FAN_ON = 9,
  G1_FAN_OFF = 10,
  G1_SHUT_DOWN = 11,
  G1_ON_ALL = 12,

};


EasyVRBridge bridge;

int8_t group, idx;

void setup()
{
  // bridge mode?
  if (bridge.check())
  {
    cli();
    bridge.loop(0, 1, 12, 13);
  }
  // run normally
  Serial.begin(9600);
  port.begin(9600);

  if (!easyvr.detect())
  {
    Serial.println("EasyVR not detected!");
    for (;;);
  }

  easyvr.setPinOutput(EasyVR::IO1, LOW);
  Serial.println("EasyVR detected!");
  easyvr.setTimeout(5);
  easyvr.setLanguage(0);

  group = EasyVR::TRIGGER; //<-- start group (customize)
  
        pinMode(8, OUTPUT); 
  digitalWrite(8, LOW);    // set the LED off
      pinMode(9, OUTPUT); 
  digitalWrite(9, LOW);    // set the LED off
      pinMode(10, OUTPUT); 
  digitalWrite(10, LOW);    // set the LED off
      pinMode(11, OUTPUT); 
  digitalWrite(11, LOW);    // set the LED off
}

void action();

void loop()
{
  easyvr.setPinOutput(EasyVR::IO1, HIGH); // LED on (listening)

  Serial.print("Say a command in Group ");
  Serial.println(group);
  easyvr.recognizeCommand(group);

  do
  {
    // can do some processing while waiting for a spoken command
  }
  while (!easyvr.hasFinished());
  
  easyvr.setPinOutput(EasyVR::IO1, LOW); // LED off

  idx = easyvr.getWord();
  if (idx >= 0)
  {
    // built-in trigger (ROBOT)
    // group = GROUP_X; <-- jump to another group X
    return;
  }
  idx = easyvr.getCommand();
  if (idx >= 0)
  {
    // print debug message
    uint8_t train = 0;
    char name[32];
    Serial.print("Command: ");
    Serial.print(idx);
    if (easyvr.dumpCommand(group, idx, name, train))
    {
      Serial.print(" = ");
      Serial.println(name);
    }
    else
      Serial.println();
    easyvr.playSound(0, EasyVR::VOL_FULL);
    // perform some action
    action();
  }
  else // errors or timeout
  {
    if (easyvr.isTimeout())
      Serial.println("Timed out, try again...");
    int16_t err = easyvr.getError();
    if (err >= 0)
    {
      Serial.print("Error ");
      Serial.println(err, HEX);
    }
                    group = GROUP_0;

  }
}

void action()
{
    switch (group)
    {
    case GROUP_0:
      switch (idx)
      {
      case G0_CLOVER:
        // write your action code here
        group = GROUP_1;// <-- or jump to another group X for composite commands
        break;
      }
      break;
    case GROUP_1:
      switch (idx)
      {
      case G1_RED_ON:
        // write your action code here
        group = GROUP_0; //<-- or jump to another group X for composite commands
                 digitalWrite(9, HIGH);    // set the LED on    
                 break;
      case G1_GREEN_ON:
        // write your action code here
        group = GROUP_0; //<-- or jump to another group X for composite commands
                 digitalWrite(10, HIGH);   // set the LED on     
                 break;
      case G1_YELLOW_ON:
        // write your action code here
        group = GROUP_0; //<-- or jump to another group X for composite commands
                 digitalWrite(11, HIGH);   // set the LED on      
                 break;
      case G1_RED_OFF:
        // write your action code here
        group = GROUP_0; //<-- or jump to another group X for composite commands
                 digitalWrite(9, LOW);   // set the LED on    
                 break;
      case G1_GREEN_OFF:
        // write your action code here
        group = GROUP_0; //<-- or jump to another group X for composite commands
                 digitalWrite(10, LOW);   // set the LED on
                 break;
      case G1_YELLOW_OFF:
        // write your action code here
        group = GROUP_0; //<-- or jump to another group X for composite commands
                 digitalWrite(11, LOW);   // set the LED on      
                  break;
      case G1_RED_BLINK:
        // write your action code here
       group = GROUP_0; //<-- or jump to another group X for composite commands
  digitalWrite(9, LOW);   // turn the LED on (HIGH is the voltage level)
  delay(1000);               // wait for a second
  digitalWrite(9, HIGH);    // turn the LED off by making the voltage LOW
  delay(1000);               // wait for a second
  
       break;
      case G1_GREEN_BLINK:
        // write your action code here
  digitalWrite(10, LOW);   // turn the LED on (HIGH is the voltage level)
  delay(1000);               // wait for a second
  digitalWrite(10, HIGH);    // turn the LED off by making the voltage LOW
  delay(1000);               // wait for a second       
         group = GROUP_0; //<-- or jump to another group X for composite commands

        break;
      case G1_YELLOW_BLINK:
        // write your action code here
  digitalWrite(11, LOW);   // turn the LED on (HIGH is the voltage level)
  delay(1000);               // wait for a second
  digitalWrite(11, HIGH);    // turn the LED off by making the voltage LOW
  delay(1000);               // wait for a second// write your action code here
        group = GROUP_0; // <-- or jump to another group X for composite commands     
        
        break;
      case G1_FAN_ON:
        // write your action code here
        group = GROUP_0;// <-- or jump to another group X for composite commands
        digitalWrite(8, HIGH);    // turn the LED off by making the voltage LOW    
        
        break;
      case G1_FAN_OFF:
        // write your action code here
       group = GROUP_0;// <-- or jump to another group X for composite commands
       digitalWrite(8, LOW);   // turn the LED on (HIGH is the voltage level)    
       
         break;
      case G1_SHUT_DOWN:
        // write your action code here
               group = GROUP_0;// <-- or jump to another group X for composite commands
               digitalWrite(8, LOW);   // turn the LED on (HIGH is the voltage level)    
               digitalWrite(9, LOW);   // set the LED on   
               digitalWrite(10, LOW);   // set the LED on
               digitalWrite(11, LOW);   // set the LED on
      case G1_ON_ALL:
        // write your action code here
               group = GROUP_0;// <-- or jump to another group X for composite commands
               digitalWrite(8, HIGH);   // turn the LED on (HIGH is the voltage level)    
               digitalWrite(9, HIGH);   // set the LED on   
               digitalWrite(10, HIGH);   // set the LED on
               digitalWrite(11, HIGH);   // set the LED on
         
        break;
      }
      break;
    }
}