Arduino Extended Database Library can't store time correctly

Dear all,

I have used the Arduino Extended Database Library to append records. Each record has different time. I have tried to output the time of two records before appending to the database. They are different. However when I output the two records, the time is the same. The time of the 1st record gets the time of 2nd record. But the other data (logid, sensor data) works fine. Here is my codes and outputs. Thanks!

#include <SPI.h>
#include <SD.h>
#include "max6675.h"
#include <SoftwareSerial.h>
#include <Wire.h>//import necessary libraries: SoftwareSerial, Wire
#include <DS3231.h>
#include "Arduino.h" 
#include <EDB.h> // for database and SD card
#define SD_PIN 4  // SD Card CS pin
//#define TABLE_SIZE 8192 // for database and SD card
#define TABLE_SIZE 10000 // for database and SD card

// Init the DS3231 using the hardware interface
DS3231  rtc(SDA, SCL);

SoftwareSerial I2CBT(9,10);//define PIN9 and PIN10 as RX and TX
int ktcSO = 2;
int ktcCS = 3;
int ktcCLK = 8;
MAX6675 ktc(ktcCLK, ktcCS, ktcSO);

const int soilMoist = 0;
// const long int recordPeriod = 43200000; // 12 hours
const long int recordPeriod = 1000;
char val; // variable to receive data from the serial port
char* db_name = "/db/edb_test.db"; // path of db files in SD card
File dbFile;  
int logid; // variable to store id of log

// Arbitrary record definition for this table.
// This should be modified to reflect your record needs.
struct LogEvent {
    int id;
    String logdate;
    String logtime;
    int temp;
    int soilmoist;
}
logEvent;

// The read and write handlers for using the SD Library
// Also blinks the led while writing/reading
void writer (unsigned long address, byte data) {
    dbFile.seek(address);
    dbFile.write(data);
    dbFile.flush();
}

byte reader (unsigned long address) {
    dbFile.seek(address);
    byte b = dbFile.read();
    return b;
}

// Create an EDB object with the appropriate write and read handlers
EDB db(&writer, &reader);

void setup() {
  
  // Open serial communications and wait for port to open:
  Serial.begin(115200);
  // Initialize the rtc object
  rtc.begin();
  // The following lines can be uncommented to set the date and time
  //rtc.setDOW(SUNDAY);     // Set Day-of-Week to SUNDAY
  //rtc.setTime(9, 1, 0);     // Set the time to 12:00:00 (24hr format)
  //rtc.setDate(31, 7, 2016);   // Set the date to January 1st, 2014
  
  I2CBT.begin(9600); //藍牙 BAUD RATE 9600
  while (!Serial) {
    ; // wait for serial port to connect. Needed for native USB port only
  }
  
  if (!SD.begin(SD_PIN)) {
      Serial.println("No SD-card.");
      return;
  }

  // Check dir for db files
  if (!SD.exists("/db")) {
      Serial.println("Dir for Db files does not exist, creating...");
      SD.mkdir("/db");
  }
  if (SD.exists(db_name)) {
      dbFile = SD.open(db_name, FILE_WRITE);
      // Sometimes it wont open at first attempt, espessialy after cold start
      // Let's try one more time
      if (!dbFile) {
          dbFile = SD.open(db_name, FILE_WRITE);
      }

      if (dbFile) {
          Serial.print(F("Openning current table... "));
          EDB_Status result = db.open(0);
          if (result == EDB_OK) {
              Serial.println(F("DONE"));
          } else {
              Serial.println(F("ERROR"));
              Serial.println("Did not find database in the file " + String(db_name));
              Serial.print(F("Creating new table... "));
              db.create(0, TABLE_SIZE, (unsigned int)sizeof(logEvent));
              Serial.println(F("DONE"));
              return;
          }
      } else {
            Serial.println("Could not open file " + String(db_name));
            return;
      }
      } else {
        Serial.print("Creating table... ");
        // create table at with starting address 0
        dbFile = SD.open(db_name, FILE_WRITE);
        db.create(0, TABLE_SIZE, (unsigned int)sizeof(logEvent));
        Serial.println("DONE");
     }    
  recordLimit();    
  deleteAll();
  
  // read sensors and append to the string:
  int sensor;
  String ltime;
  sensor = analogRead(soilMoist);
  logEvent.id = logid;
  logid = db.count()+1;
  //logEvent.logdate  = rtc.getDateStr();
  logEvent.logtime = rtc.getTimeStr();
  Serial.println("TIME"+logEvent.logtime);
  logEvent.soilmoist  = sensor;
  logEvent.temp =  int(ktc.readCelsius()); // temperature sensor data
  EDB_Status result = db.appendRec(EDB_REC logEvent);
  if (result != EDB_OK) printError(result);
  Serial.println(F("Append 1 record"));    
  delay(5000); 
  // read sensors and append to the string:
  sensor = analogRead(soilMoist);
  logEvent.id = logid;
  logid = db.count()+1;
  //logEvent.logdate  = rtc.getDateStr();
  logEvent.logtime = rtc.getTimeStr();
  Serial.println("TIME"+logEvent.logtime);
  logEvent.soilmoist  = sensor;
  logEvent.temp =  int(ktc.readCelsius()); // temperature sensor data
  result = db.appendRec(EDB_REC logEvent);
  if (result != EDB_OK) printError(result);
  Serial.println(F("Append 1 record"));    
  delay(5000); 
  selectAll();
  dbFile.close();
}

void loop() {
  // make a string for assembling the data to log:
  String dataString = "";
 
  byte cmmd[20]; 
  int insize; 
    
  if ((insize=(I2CBT.available()))>0)
  {  //判斷有沒有訊息接收 
    dataString += String(insize);
    dataString += ",";
     for (int i=0; i<insize; i++) {
       cmmd[i]=char(I2CBT.read());//將接收的訊息顯示出來
       dataString += cmmd[i];
       dataString += ",";
     }
  } 
  delay(1000); 
   
}

void recordLimit()
{
    Serial.print(F("Record Limit: "));
    Serial.println(db.limit());
}

void countRecords()
{
    Serial.print(F("Record Count: "));
    Serial.println(db.count());
}

void printError(EDB_Status err)
{
    Serial.print(F("ERROR: "));
    switch (err)
    {
        case EDB_OUT_OF_RANGE:
            Serial.println(F("Recno out of range"));
            break;
        case EDB_TABLE_FULL:
            Serial.println(F("Table full"));
            break;
        case EDB_OK:
        default:
            Serial.println(F("OK"));
            break;
    }
}

void selectAll()
{
    for (int recno = 1; recno <= db.count(); recno++)
    {
        EDB_Status result = db.readRec(recno, EDB_REC logEvent);
        if (result == EDB_OK)
        {
            Serial.print(F("Recno: "));
            Serial.print(recno);
            Serial.print(F(" ID: "));
            Serial.print(logEvent.id);
            //Serial.print(F(" Date: "));
            //Serial.print(logEvent.logdate);
            Serial.print(F(" Time: "));
            Serial.print(logEvent.logtime);
            Serial.print(F(" Temp: "));
            Serial.println(logEvent.temp);
            Serial.print(F(" Soil Moisture: "));
            Serial.println(logEvent.soilmoist);
        }
        else printError(result);
    }
}

void deleteAll()
{
    Serial.print("Truncating table... ");
    db.clear();
    Serial.println("DONE");
}

The output is as follows.

TIME14:55:13

Append 1 record

TIME14:55:19

Append 1 record

Recno: 1 ID: 0 Date: Time: 14:55:19 Temp: 22

Soil Moisture: 1009

Recno: 2 ID: 1 Date: Time: 14:55:19 Temp: 22

Soil Moisture: 1022

Surely that is not your complete code?

I don’t see your definition of the DB record, nor where you open the database.

Is there more? It may be helpful to see all of it.