Arduino External Clock Electric Specs?

I need to clock an Arduino Pro Mini 328 (3.3V) at 10 MHz using an LPRO Rubidium Oscillator. I can’t find the electrical specs for the External Clock on the 328.

The specs for the LPRO are:

10 MHz sine-wave

.55 Vrms +/- .05 Vrms into

50 ohm [+7.8 +/- 0.8 dBm]

Any help would be appreciated!

thanks,

glenn

http://www.avrfreaks.net/index.php?name … 736#643736

MBedder

PostPosted: Dec 01, 2009 - 01:19 AM

Location: Zelenograd, Russia

Set the CKSEL to 0111 (Full swing xosc) and feed your LPRO output to XTAL1 pin via the 1…10 nF capacitor. Check the XTAL2 output with an scope - you should get a clean and almost square waveform out there which indicates the Mega is clocked properly.

This trick makes an amplifier out of the XTAL1->XTAL2 invertor which is self biased to a linear gain region due to an internal feedback resistor which is connected only in internal crystal CKSEL modes.

–

I’ll be testing this soon and posting the results!

-glenn

Rubidium oscillator, something I haven’t had a chance to play with :).

Have a link?

LPROs were the first atomic frequency standard designed for mass production by Efratom (then Datum, now Symmetricom). They have a design life of 20+ years. New, they were about $2,250 + $250 for a warranty (IIRC). Now, they can be had for <$100 on ebay:

http://shop.ebay.com/?_from=R40&_trksid … Categories

They have been replaced by the XPRO:

http://www.symmetricom.com/products/fre … dard/XPRO/

Design notes:

-run on ~24 volts dc

-use 15-20 watts

-have a built-in test indicator (BITE) (aka “Lock”)

-fit in 1U rack mounts

-electrical and mechanical c-field control (neither usually needed)

You just cost me $80 :shock: