I’m a rookie Arduino user, and I want to make sure I’m getting all the necessary components for this project in the first go around.
The goal is to read in a voltage, transmit that reading wirelessly to a computer and then write it to serial.
If I’m using the ardiono fio, I need 2 Xbee antennaes and a USB Explorer Dongle to actually do the project, right?
Specifically, I was looking at these products.
http://www.sparkfun.com/commerce/produc … ts_id=9819
http://www.sparkfun.com/commerce/produc … ts_id=8665
Thanks.
waltr
2
Those XBees should do just fine. You may want to add in an XBee breakout board to make wiring to the XBee easier.
http://www.sparkfun.com/commerce/produc … ts_id=8276
or the Regulated explorer that includes a 3.3V regulator:
http://www.sparkfun.com/commerce/produc … ts_id=9132
I’m going to be using a 3.6 V battery so is the explorer board still necessary?
Thanks for your help.
stevech
4
I’d recommend you ensure that you order XBee series 1, not 2. And decide if you need the higher transmit power of the XBee Pro.