I have been using the Arduino IDE ver 1.67 to develop a demo using the qduino mini. I didn’t change or update anything but suddenly I can no longer compile a previously working project with the following error:
"Arduino: 1.6.7 (Windows 7), Board: “Qduino Mini”
Board qduinomini (platform avr, package SparkFun) is unknown
Error compiling."
I selected Tools and the Board and found that none of the sparkfun boards were listed anymore. I launched the Boards Manager and scrolled to the Sparkfun AVR boards and saw that I could select Install, so I did. The sparkfun boards were not listed in the boards list so I selected the Qduino Mini again but I still can’t compile even though the manager shows Sparkfun AVR Boards by Sparkfun Electronics version 1.1.4 INSTALLED is listed.
I can load an example sketch for the Qduino but it displays the same error message posted above.
Any help would be appreciated. Also, what can change in the IDE without my intervention???
I did make one, change. I connected a second qduino mini since the first was working well. Are there different versions of the preloaded firmware available, and can that affect the IDE???
update — I found that I can’t select ANY sparkfun arduino boards. They all fail compile with the same error. Apparently the sparkfun driver has failed somehow even though the board manager states it’s installed.
Thanks,
Dan