i have an arduino + lcd keypad and i want to put a function in a case menu but i dont know how .the function must count how many times i push a button in a period of time.i use pin 2 and 3 for buton.if somebody can help me with the cod.please help me. thanx a good day.
the cod for my menu is:
#include <LiquidCrystal.h>
// Initialize the library with the numbers of the interface pins
LiquidCrystal lcd(8, 9, 4, 5, 6, 7);
//States for the menu.
int currentMenuItem = 0;
int lastState = 0;
void setup() {
//Set the characters and column numbers.
lcd.begin(16, 2);
//Print default title.
clearPrintTitle();
}
void loop() {
//Call the main menu.
mainMenu();
}
void mainMenu() {
//State = 0 every loop cycle.
int state = 0;
//Refresh the button pressed.
int x = analogRead (0);
//Set the Row 0, Col 0 position.
lcd.setCursor(0,0);
//Check analog values from LCD Keypad Shield
if (x < 100) {
//Right
} else if (x < 200) {
//Up
state = 1;
} else if (x < 400){
//Down
state = 2;
} else if (x < 600){
//Left
} else if (x < 800){
//Select
state = 3;
}
//If we are out of bounds on th menu then reset it.
if (currentMenuItem < 0 || currentMenuItem > 4) {
currentMenuItem = 0;
}
//If we have changed Index, saves re-draws.
if (state != lastState) {
if (state == 1) {
//If Up
currentMenuItem = currentMenuItem - 1;
displayMenu(currentMenuItem);
} else if (state == 2) {
//If Down
currentMenuItem = currentMenuItem + 1;
displayMenu(currentMenuItem);
} else if (state == 3) {
//If Selected
selectMenu(currentMenuItem);
}
//Save the last State to compare.
lastState = state;
}
//Small delay
delay(5);
}
//Display Menu Option based on Index.
void displayMenu(int x) {
switch (x) {
case 1:
clearPrintTitle();
lcd.print (“->TESTARE BATRANI”);
break;
case 2:
clearPrintTitle();
lcd.print (“->TESTARE TINERI”);
break;
case 3:
clearPrintTitle();
lcd.print (“->TESTARE COPII”);
break;
}
}
//Print a basic header on Row 1.
void clearPrintTitle() {
lcd.clear();
lcd.setCursor(0,0);
lcd.print(“MENU TESTER”);
lcd.setCursor(0,1);
}
//Show the selection on Screen.
void selectMenu(int x) {
switch (x) {
case 1:
clearPrintTitle();
lcd.print (“Selectat TEST BATRANI”);
//Call the function that belongs to Option 1
break;
case 2:
clearPrintTitle();
lcd.print (“Selectat TEST TINERI”);
//Call the function that belongs to Option 2
break;
case 3:
clearPrintTitle();
lcd.print (“Selectat TEST COPII”);
//Call the function that belongs to Option 3
break;
}
}