Arduino Pro 3.3V 8Mhz

Hi,

I want to know why I am unable to access via the ICSP the Arduino Pro which runs at 3.3v and 8Mhz purchased from the website. I used the avrispmkii and the AVR Studio 4 with the SP3.

The error output displayed shows:

‘There seems to be a short circuit on the ISP connector. The MOSI line(s) appear to be short-circuited. The operation will be aborted.’

This happens when I try to read the Signature. However, I am able to download via the FTDI the code. I just want to get access with the ICSP because I am working with a fyi pcb which integrates the same circuit and I having the same error. BTW, I used two avrisp just in case the programmer was the problem.