Hi everyone,
I want to control a frequency inverter with Arduino UNO. I only need START/STOP.
I have chosen the ALsw- configuration (pages 20-21 from Manual): So, I placed a N channel Mosfet 2N7000 (GATE to output 11 Arduino, SOURCE to GND Arduino, DRAIN to PIN 1 inverter). Moreover, I have a R=10K between GATE and SOURCE. Finally, PIN 4 from inverter is connected to GND Arduino. (I attach the connections)
http://oi60.tinypic.com/otnn6x.jpg
http://oi60.tinypic.com/14vpnpj.jpg
http://oi61.tinypic.com/152gnth.jpg
Then I wrote this code to check the start/stop with a digital input:
int comandar=11;
void setup()
{
pinMode(comandar, OUTPUT);
}
void loop()
{
digitalWrite(comandar, HIGH);
delay(2000);
digitalWrite(comandar, LOW);
delay(2000);
}
The problem is… It doesn´t work.
The inverter parameters that I changed are:(pages 26 and 30 from inverter manual)
P100: Start control source = 1 (Terminal strip: Use start/stop circuit wired into the terminal strip)
P120: Assertion level = 1(LOW)
What did I do wrong? I suppose I need to change another parameters ¿?
Any idea?
Thank you in advance
Best regards](EMW e-commerce)