Hi everyone,this is my first post to this forum.
I want to drive four DC motor for my robot project.
I found Ardumoto is the best for driving motor with Arduino Uno.
But it can only drive 2 motor.
Can i use two motor driver(2x shield)?
I found the shield use digital 12, pwm 3, digital 13 and pwn 11 to drive these two motors.
Is it possible if I adding another shield on to the first shield (Is it(second) use the same pins to drive another two motors).
And I also want to use Xbee shield.
Thanks
John ![]()