Hey guys,
Here’s what I’ve got:
one of these (xbee pro series 2, chip mount antenna)
http://www.sparkfun.com/commerce/produc … ts_id=8767
mounted on one of these (usb serial adaptor)
http://www.sparkfun.com/commerce/produc … ts_id=8687
trying to communicate with one of these (arduino xbee)
http://www.sparkfun.com/commerce/produc … ts_id=8471
mounted on one of these (arduino usb board)
http://www.sparkfun.com/commerce/produc … cts_id=666
I pulled the AVR from the arduino and flipped the xbee/usb jumpers so that it is just a serial pass-through.
I can hook up both to X-CTU and a terminal emulator without a problem.
Initially, the xbee on the arduino was set up with the “Zigbee Router/Endpoint Device AT” feature set.
The xbee pro was setup with the “ZNET 2.5 Router/Endpoint Device AT” feature set.
No matter what I did with the destinations, channels, etc I could not get the two to communicate. I assumed the problem was with the feature set, so I reflashed the arduino Xbee to the ZNET feature set and tried again.
I’m still striking out. I only get “ERROR” in reply when I do any node discovery. Neither device is sleeping and I’m not sure what else to check.
Anyone have any advice? Is there a problem with using an Xbee and an Xbee pro?
Thanks