Hello,
My first post. Apologies if this is not the correct place to post this topic or not enough information.
I recently purchased the Benewake TFMini-S LIDAR unit and the Sparkfun Redboard Artemis. I am having some trouble getting Serial2 to communicate with the TFMini-s and wanted to know if there was an existing Sketch for communicating between these two devices. I am having issued with the Serial2 in the TFMP_example.ino Sketch.
My main issue seems to be that I can talk fine to the Serial port using the Serial.ino sketch but cannot talk to the TFmini-S on the TX1-RX1 pins on the Redboard Artemis Itried Serial2 and Serial1). I am trying to use HardwareSerial since the Redboard Artemis has two UARTs and not SoftwareSerial.
Thanks
Maybe your issue is this known issue https://github.com/sparkfun/Arduino_Apollo3/issues/349. It is serial1 to use.
Thank you Paulvha. I appreciate your response.
Could you point me to some Sketch that is making use of the RX1/TX1 pins on the Redboard Artemis? I am new to this world and I could be missing something simple.
Thank you again.
void setup()
{
Serial1.begin(115200);
Serial.begin(115200);
}
void loop()
{
if (Serial.available())
{ // If data comes in from serial monitor, send it out to TX1
Serial1.write(Serial.read());
}
if (Serial1.available())
{ // If data comes in from RX1, send it out to serial monitor
Serial.write(Serial1.read());
}
}
Jumper RX1 and TX1 and anything you send at 115200 baud should echo back to you.
Thank you YellowDog. I appreciate it. Can you please let me know what include files to place at the top? I think this might be where I am going wrong.
Thanks again
No include files needed, that code example will work as is.