ARM7 Development boards question...

Hi all,

I need to get a proto/dev board for the following ARM uP

“1891 SAM7s 56”

I’m not familier with the ARM processors, so I’m not sure the exact board to get…

Any suggestions?

Thanks!

~Kam (^8*

oops,

I mean “AT91SAM7S256” dev boards…

~Kam (^8*

Hi,

You should be more specific with what you want to do with it. The AT91SAM7S256 is an good all rounder with USB, CAN bus, SPI, I2C, etc. It’s best to choose between the an LPC from Philips or SAM from Atmel since these are these have the most support software for ARM7. For instance I choose rather for an LPC2148 instead of the allmost similar AT91SAM7S256, cause there more software was avialable for this device regarding USB. If you would want an all rounder then I would advise you to choose between an AT91SAM7S256 or LPC2148. The only thing is that they pretty much don’t support is Ethernet.

Have fun

Rhino:
Hi,

You should be more specific with what you want to do with it.


Werty said :

Yes , many uses of EVB because of bad software/firmware

criipples MCU .

If we had powerful s/w , we could simply use MCU at high

level , for fun , get on with our lives … :smiley:

Everything , starting with ARM Loader , must be

improved , so we can get on with higher level

programming .

I am doing a new Loader with a new

Forth . It will eliminate Linux .

Forth extends from loader , into

PSRAM_SIZE_8 .

Notice my notation ! Its unambigous and

proceedural and ordinal .

It is temporary , because my Forth

will use true GUI , and no text .

Program computers with

No Text and No English …


BTW M$ OutHouse_Express was the only

method to pass Virus .

Switching to WebMail stopped all Virus .

Thanks 8) Bill Gates , for Virus .

Hotmail , Yahoo , Google sell your email address

to Junk mail .

All advertizers do this !

People who deny , are the very ones making

the money !!

Stay tuned , soon free ARM S/W

wertywertywerty at swissinfoswissinfoswissinfo

orgorgorgorgorg