Hi,
having used the Artemis Nano in the past, now coming back to it after a year and nothing compiles anymore. I can upload Blink no problem but most of everything else is an issue and won’t compile, most importantly I want to run motors and just using the MotorTest.ino file already gives me this error below.
I updated all the boards and libraries and keep getting this error:
{…}Serial_Controlled_Motor_Driver\src\SCMD.cpp: In member function ‘uint8_t SCMD::begin()’:
{…}Serial_Controlled_Motor_Driver\src\SCMD.cpp:106:7: error: ‘class arduino::MbedSPI’ has no member named ‘setClockDivider’
SPI.setClockDivider(SPI_CLOCK_DIV32);
^~~~~~~~~~~~~~~
{…}Serial_Controlled_Motor_Driver\src\SCMD.cpp:106:23: error: ‘SPI_CLOCK_DIV32’ was not declared in this scope
SPI.setClockDivider(SPI_CLOCK_DIV32);
^~~~~~~~~~~~~~~
{…}Serial_Controlled_Motor_Driver\src\SCMD.cpp:108:7: error: ‘class arduino::MbedSPI’ has no member named ‘setBitOrder’
SPI.setBitOrder(MSBFIRST);
^~~~~~~~~~~
{…}Serial_Controlled_Motor_Driver\src\SCMD.cpp:111:7: error: ‘class arduino::MbedSPI’ has no member named ‘setDataMode’
SPI.setDataMode(SPI_MODE0);
any help is appreaciated.
Chris