Hi.
I have a project that was using a RedBoard (328P/UNO style) without a problem, and now I’m building its sister project using a RedBoard Artemis, and running into issues with the SparkFun Qwiic Motor Driver when trying to compile Arduino code for it.
Using Arduino IDE 2.1.0, I open up the example sketch “MotorTest.ino” from the Serial Controlled Motor Driver library (v1.04), choose the RedBoard Artemis Nano (I’ve got v2.2.1 of SparkFun Apollo3 Boards installed). When I hit compile I get the following errors, seemingly related to SPI (which I’m not using, I’m using the example sketch as is, in I2C mode)…
/Documents/Arduino/libraries/Serial_Controlled_Motor_Driver/src/SCMD.cpp: In member function 'uint8_t SCMD::begin()':
/Documents/Arduino/libraries/Serial_Controlled_Motor_Driver/src/SCMD.cpp:106:7: error: 'class arduino::MbedSPI' has no member named 'setClockDivider'
   SPI.setClockDivider(SPI_CLOCK_DIV32);
       ^~~~~~~~~~~~~~~
/Documents/Arduino/libraries/Serial_Controlled_Motor_Driver/src/SCMD.cpp:106:23: error: 'SPI_CLOCK_DIV32' was not declared in this scope
   SPI.setClockDivider(SPI_CLOCK_DIV32);
                       ^~~~~~~~~~~~~~~
/Documents/Arduino/libraries/Serial_Controlled_Motor_Driver/src/SCMD.cpp:108:7: error: 'class arduino::MbedSPI' has no member named 'setBitOrder'
   SPI.setBitOrder(MSBFIRST);
       ^~~~~~~~~~~
/Documents/Arduino/libraries/Serial_Controlled_Motor_Driver/src/SCMD.cpp:111:7: error: 'class arduino::MbedSPI' has no member named 'setDataMode'
   SPI.setDataMode(SPI_MODE0);
       ^~~~~~~~~~~
exit status 1
Compilation error: exit status 1
If I change the board target to the old SparkFun Redboard, it compiles without a problem.
If been digging for information for a few hours now, but not coming up with anything useful. Any ideas?