Hi, everyone, I’ve been trying to upload code to the Artemis, with no success. This is what I’ve tried so far:
Using the Arduino IDE and the SVL bootloader, this is the error:
[10896] Failed to execute script artemis_svl
Traceback (most recent call last):
Artemis SVL Bootloader
File "artemis_svl.py", line 393, in <module>
File "artemis_svl.py", line 331, in main
phase: setup
File "artemis_svl.py", line 176, in phase_setup
cleared startup blip
File "artemis_svl.py", line 132, in wait_for_packet
phase: bootload
IndexError: index out of range
have 7464 bytes to send in 4 frames
error receiving packet
{'len': 0, 'cmd': 0, 'data': 0, 'crc': 1, 'timeout': 1}
unknown error
sending frame #0, length: 0
Upload failed
phase: setup
cleared startup blip
el puerto seleccionado cleared startup blip
no existe o tu placa no esta conectada
The last error lines mean “The selected port cleared startup blip does not exist or the board is not connected.”
When using the Makefile to load the sketch the infamous port-is-currently-open error appears:
Artemis SVL Bootloader
phase: setup
cleared startup blip
phase: bootload
have 13240 bytes to send in 7 frames
error receiving packet
{'len': 0, 'cmd': 0, 'data': 0, 'crc': 1, 'timeout': 1}
unknown error
sending frame #0, length: 0
Upload failed
phase: setup
cleared startup blip
/dev/ttyUSB0 is currently open. Please close any other terminal programs that may be using /dev/ttyUSB0 and try again.
If using bootloader_asb, the errors are:
Arduino IDE
[18321] Failed to execute script ambiq_bin2board
Traceback (most recent call last):
File "ambiq_bin2board.py", line 24, in <module>
ModuleNotFoundError: No module named 'am_defines'
ModuleNotFoundError: No module named 'am_defines'
Makefile
Makefile:126: warning: you have not defined SDKPATH so will continue assuming that the SDK root is at ../../../../..
Makefile:134: warning: you have not defined COMMONPATH so will continue assuming that the COMMON root is at ../../../../common
Makefile:142: warning: you have not defined BOARDPATH so will continue assuming that the BOARD root is at ../../..
Makefile:150: warning: you have not defined PROJECTPATH so will continue assuming that the PROJECT root is at ..
/usr/bin/python3 ../../../../common/tools_sfe/ambiq/ambiq_bin2board.py --bin bin/example_asb.bin --load-address-blob 0x20000 --magic-num 0xCB -o bin/example --version 0x0 --load-address-wired 0xC000 -i 6 --options 0x1 -b 115200 -port /dev/ttyUSB0 -r 2 -v
Header Size = 0x80
original app_size 0x33b8 ( 13240 )
load_address 0xc000 ( 49152 )
app_size 0x33b8 ( 13240 )
w0 = 0xcb003438
Security Value 0x10
w2 = 0x10008080
addrWord = 0xc000
versionKeyWord = 0x0
child0/feature = 0xffffffff
child1 = 0xffffffff
crc = 0x944f7ce5
Writing to file bin/example_OTA_blob.bin
testing: bin/example_OTA_blob.bin
Header Size = 0x60
app_size 0x3438 ( 13368 )
Writing to file bin/example_Wired_OTA_blob.bin
Image from 0x0 to 0x3438 will be loaded at 0x20000
Connecting over serial port /dev/ttyUSB0...
Sending Hello.
Received response for Hello
Received Unknown Message
msgType = 0x0
Length = 0x0
['0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0']
Fail
Sending Hello.
Received response for Hello
Received Unknown Message
msgType = 0x0
Length = 0x0
['0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0']
Fail
Sending Hello.
Received response for Hello
Received Unknown Message
msgType = 0x0
Length = 0x0
['0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0', '0x0']
Fail
Tries = 3
Upload failed
I’ve tested everything I found in forums and webs for days, and anything seems to work.
Also, I find strange that the result varies depending on the method. I’ll keep investigating.
In anyone could help, I’d be really grateful ![]()
Cheers,
David.