AS1130

I’ve found this great IC from austriamicrosystems

Its the AS1130 and its a 132 LED driver which comes in a 28-pin SSOP package, and I would love to be able to use it but I can’t figure out which pins are necessary and all that, I think you guys understand it way more than I do. Please can you make a breakout for it so I can get to making the most awesome LED stuff that humanity and all lifeforms across the universe shall see.

Me love you long time if this happens

Hi Lefty,

if you just have problems with software: a brief software for AS1130 LED driver is already available:

http://dl.kokosnuss.org/

http://dl.kokosnuss.org/as1130_test.ino

as we are working on a clock using the AS1130:

https://groups.google.com/group/qlocktw … e26f7dbf06

Also since it seems you dont know in detail how the AS1130 is working this link might be useful:

http://www.digikey.de/PTM/PTMPartList.p … &ptm=25773

It explains very basically how the crossplexing is done.

If you are asking for a shield, this would be a nice idea as it is a great LED driver, but only available in SSOP-28

BTW: free samples are here

http://www.austriamicrosystems.com/AS1130

Br.

Wow thank you!