I’m attempting to get my new AS3935 to work with a D1 Mini, using ESPHome’s SPI & AS3935_SPI modules.
The Wemos boots fine and firmware installed when no As3935 is connected. I’ve double-checked the connections and then wrote them down (below)to make sure I wasn’t mis-wired and I’m 98% sure I’m on track there.
If I remove the “CS” line, it boots up… but with everything connective, I get no response upon power-on or reset.
Connections are:
AS3935 - Wemos D1 Mini Wiring
AS3935 - wire - D1 Mini
-------------------------------
mosi - purple - d7 (GPIO13, MOSI)
miso - blue - d6, (GPIO12, MISO)
sck - green - d5 (GPIO14, SCLK)
cs - grey - d8 (GPIO15, CS)
int - red - d1 (GPIO5)
3v3 - white - 3v3,
gnd - brown - G
and the relevant ESP code is here:
spi:
# clk_pin: D5
# mosi_pin: D7
# miso_pin: D6
clk_pin: GPIO14
mosi_pin: GPIO13
miso_pin: GPIO12
as3935_spi:
# cs_pin: D8
cs_pin: GPIO15
# irq_pin: D1
irq_pin: GPIO5
indoor: true
noise_level: 2
spike_rejection: 2
# lightning threshold (default 5) can be: 1, 5, 9, or 16. number of lightnings that must appear in a 15-minute time window before a lightning storm is detected
lightning_threshold: 5
mask_disturber: false
div_ratio: 0
capacitance: 0
# watchdog threshold (default 2)
watchdog_threshold: 1
Could this just be as simple as “it’s a bad board” ? Or is there something I need to invert for the CS line?
Hmmmm, have you managed to get the lightning sensor working with a different controller closer to what our hook-up guide suggests? An Arduino Uno board or similar should work.
Have you managed to get the SPI interface of the ESP8266 D1 mini working on a different device? I can’t really offer much in support on the product because we do not carry it, however, I do know that ESP devices can be a bit finicky to work with in general.