Hello Sparkfun forum,
Although the Tiny Programmer 11801 has been used successfully
a couple of times before, today after the sketch is compiled in Arduino IDE V 2.3.5, when the sketch is sent to the Tiny Programmer the IDE returns:
"Failed programming: uploading error: exit status 1 "
The setup to sending the sketch is:
Win-11 USB port and the Ardino IDE set to Board: ATTiny…85, Processor: ATtiny85, Clock: Internal 1MHz and Programmer: USasp (Attiny CoreBtiny)
After the setup at “Tools” at the “Sketch” tab the “Upload Using Programmer” option is chosen.
Have tried several times with same result.
Thanks.
Allen Pitts
Try selecting USBTinyISP instead and see how that goes (if not, also try swapping ports/cables)
Hello TS-Russell and the Sparkfun forum,
Tried selecting the USBTinyISP. It worked once then subsequent attempts to upload to the Atttiny using Arduino IDE V 2.3.5, when the sketch is sent to the Tiny Programmer the IDE returns:
"Failed programming: uploading error: exit status 1 "
I have two Sparkfun Tiny Programmer 11801. Neither work.
Tried different ATtinies. Tried different ports. Tried different cables.
Tried plugging the Tiny Programmer directly into the USB on
the laptop. Tried different sketches like the Blink sketch in the
IDE Examples.
Attached is a screen shot of the set up at the Arduino IDE Tools tab.
The various articles and tutorials like
have been scoured for hours but no solution can be found,
I am dead in the water until I can get the sketch uploaded to
the microcontroller.
Thanks.
Allen Pitts
PS Attached is screenshot of the setu
p at the IDE > Tools > chosen before Sketch > Upload Using Programmer is chosen
An alternative might be to try downloading the legacy Arduino IDE (1.8x, on their site) and install to a different drive/folder and try it, I’ve had a bit more luck with it vs the newer IDE & toolchain