So, I’m going through the first set of tutorials, I’ve created my nice 5v supply and plugged in my atmega328p into the breadboard, wire it all up and hopefully ready to start programming it with the pocket programmer.
My confusion lies in that the programmer seems to provide it’s own ~5v supply (via the USB) such that when I plugged it into the board it lit up my first LED. Ah I thought, noob error I have the switch on the programmer flicked to “Power Target”, so I switched it to “No Power”. All that did was slightly reduce the output voltage, still the LED continue :? d to light.
So I’m in a pickle, what’s the process for getting the AVR Pocket Programmer to work with the breadboard?
-
Do I let it power the system through the USB?
-
Is the “No Power” switch not working?
-
Can I safely have the VCC and GND connections all hooked up and still power the board via the “wall wart”?
-
Should I give up and go back to licking windows?
Any help will be greatly appreciated as I’m completely new to this micro-controller Lark. Thanks.