WTF is the device that I give after the “-P” option to avrdude? Olimex claims it’s a USB CDC device, so it “doesn’t need drivers”. So what, exactly, should I expect to see in /dev? I’ve got nothing named usb or USB anything, and the only “cu” devices are for cell phones. I’ve been Googling away, no answer yet.
I went through this same song and dance with PIC programmers, this looked more promising from the docs, but it’s not looking so good now.
AHA.
Following the mention of “updated firmware drivers (installed from a PC)” ( viewtopic.php?t=13839 ) I borrowed my wife’s computer (Mac with VMWare with XP) and te-di-ous-ly installed the drivers and the firmware upgrade software. Christmas, this is slow.
And with the driver installed, the updated installed and running, pins 1 and 3 shorted, light blinking red/green just as the doc describes, it’s not working. not COM1, not COM2, not COM3.
I made my way to device manager, verified that every single setting matched what was described in the doc, ensured that it was COM3, and it Did Not Work.
Is it too much to ask, if a device is claimed to support a Macintosh, that it is actually tested on a Macintosh?