Hi,
I’m new in ARM world and i have some problems on setting up environment. I tried to follow the yagarto howto but different hw is used so had to impro.
First problem is that i tried to conf the openocd with config file
#daemon configuration
telnet_port 4444
gdb_port 3333
#interface
interface ft2232
ft2232_device_desc "Olimex OpenOCD JTAG A"
ft2232_layout "olimex-jtag"
ft2232_vid_pid 0x15BA 0x0003
jtag_speed 2
#use combined on interfaces or targets that can't set TRST/SRST separately
reset_config trst_and_srst srst_pulls_trst
#jtag scan chain
#format L IRC IRCM IDCODE (Length, IR Capture, IR Capture Mask, IDCODE)
jtag_device 4 0x1 0xf 0xe
#target configuration
daemon_startup reset
#target <type> <startup mode>
#target arm7tdmi <reset mode> <chainpos> <endianness> <variant>
target arm7tdmi little run_and_halt 0 arm7tdmi-s_r4
run_and_halt_time 0 30
# commands below are specific to AT91sam7 Flash Programming
# ---------------------------------------------------------
#target_script specifies the flash programming script file
target_script 0 reset c:\scriptTemp\temp.ocd
#working_area <target#> <address> <size> <'backup'|'nobackup'>
working_area 0 0x40000000 0x4000 nobackup
#flash bank at91sam7 0 0 0 0 <target#>
flash bank at91sam7 0 0 0 0 0
# For more information about the configuration files, take a look at:
# http://openfacts.berlios.de/index-en.phtml?title=Open+On-Chip+Debugger
when i try when card is connected:
C:\Program Files\openocd-2006re115\bin\configs>openocd-ftd2xx -f at91sam7_armusb
ocd.cfg
Info: openocd.c:82 main(): Open On-Chip Debugger (2006-10-12 18:00 CEST)
Warning: arm7_9_common.c:683 arm7_9_assert_reset(): srst resets test logic, too
after that i have to use ctrl+break it to stop or reset console…
and if just arm-usb-ocd is connected:
C:\Program Files\openocd-2006re115\bin\configs>openocd-ftd2xx -f at91sam7_armusb
ocd.cfg
Info: openocd.c:82 main(): Open On-Chip Debugger (2006-10-12 18:00 CEST)
Error: jtag.c:1149 jtag_validate_chain(): Error validating JTAG scan chain, IR
mismatch, scan returned 0x00
I dont know if my second problem cose of openocd but if i try in eclipse make it gives like make: *** No rule to make target clean'. or make: *** No rule to make target all’.
Is there some problem with my make too.
Thanks for help in advance
- Wicim