Hi All,
i have newly purchased a OLIMEX SAM7 - EX256 .
I am facing some problems , actually severe issues with it :(( .
Configuration:
Board – SAM7 - EX256
JTAG – ARM JTAG by OLIMEX
These are the things that i am facing .
Problem:
– when i tried to connect the HJTAG tool it always tells me Unable to detect target.
– And the same is true when i try to connect OCD software also.
– The board had initially booted up with only the “OLIMEX” logo in the LCD.I accidently shorted the ERASE pins and i guess i erased the Flash.After that the board boots up (i come to know when the USB connected notification comes in my PC ) only when the JTAG pin is shorted but no more LCD display.
Is there a BSL pin the above mentioned board ?? which i can short (as mentioned in the ARM development material for Eclipse).
PLease help me out of this tricky situation.
rgds
som