Hi all,
I’m working on a camera design using a PIC to interface to a CMOS image sensor and I have a few questions about the best way to design/make a breakout board for the CMOS IC.
Basically i have to options, firstly i can just do a straight pin breakout where i run each pin on the chip to a header on the board and turn the IC into a 48pin DIL.
Alternately i could make a board that exposes just the pins i want and has all the voltage regulators and decoupling caps required already in place so i can just go straight to using it.
The first one is obviously much simpler and would require all the voltage regulators off the board ( i need 2.8 and 1.8 volts )
The second is more compact and more educational ( i’ll learn more about layouts and general circuit design from it ).
I’m torn between my two general engineering principles. Keep It Simple, and Keep It Neat.
Does anyone have any other pros/cons/general opinions that could help me formulate my decision? If it werent for the fact that the CMOS IC is fairly expensive (£16) and is going to be a bitch to solder (all the pins are below the chip) i’d just make both for the experience.