Billing Q

The page says round up to the nearest inch but it is not explicit about linear inch or sq inch. if my design is 1.1"x1.1" is that 22=4 inches i pay for or is it 1.11.1 = 1.21 = 2 inches?

See [this thread.

Don](http://www.sparkfun.com/cgi-bin/phpbb/viewtopic.php?t=749)

ct:
The page says round up to the nearest inch but it is not explicit about linear inch or sq inch. if my design is 1.1"x1.1" is that 22=4 inches i pay for or is it 1.11.1 = 1.21 = 2 inches?

Figure out square inches first and then round up to the nearest whole number.

1.1 x 1.1 = 1.21 rounded up = 2 square inches

-Bill