You state that the minimum billable size is 1" x 1". Is this the actual square area or are you stating that each dimension is billable in 1" increments? For instance I have a board which is 0.8" x 1.2" inches, is this billable as a 1 sq in or 2 sq in board? If it is the latter do you permit panalized submittal (2 boards in 1 submission whose agregate size is 2" x 1")?
Take the with and multiply by height and then round up to nearest inch. Thats what u pay for.
So 0.8 x 1.2 = 0.96 = 1 square inch
What about if we were submitting say 10 boards, each of which the area was 0.5sq in. Would 10 boards be billed as 10 sq in or as 5 sq in?
See [[this post](http://www.sparkfun.com/cgi-bin/phpbb/viewtopic.php?t=756) from Nathan.Tre:
What about if we were submitting say 10 boards, each of which the area was 0.5sq in. Would 10 boards be billed as 10 sq in or as 5 sq in?
Don](http://www.sparkfun.com/cgi-bin/phpbb/viewtopic.php?t=756)
Exactly what I was looking for, thanks!